Part Number: INA700-701EVM
Other Parts Discussed in Thread: INA239, TI-SCB, INA700
This issue seems to be similar to another EVAL + SCB thread: "INA239: EVM/SCB Connect Fail". Following the instructions - installed the PAMB drivers as administrator, updated the firmware via the GUI, and tried to connect. I am encountering a myriad of issues even though the MSP432 Bulk device and the MSP432 USB serial port (COM5) show up in the device manager. I did also force another FW update by putting the SCB into DFU mode since that was suggested in the aforementioned thread. The green LED goes out and I did see "Flash Successful" after. Still encountering the following:
1) ERROR - Hardware not connected. Cannot open serial port: COM5
2) Connection Failure - No SCB controller detected
3) Disconnect SCB for 10 sec, reconnect: At bottom of screen "Connected to SCB Controller, but failed to connect to SCB w/TI_SCBEVM, FW: v1.1.0.0on DEFAULT". An then in the middle of the screen - Connection Failure - ERROR: Connection to bulk device timed out
4) If I click the reconnect button on the lower left, "Connecting to target..." along with a moving progress ribbon is displayed for several minutes ending with the ERROR...COM5 message shown above.