This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC is like wear debris sensor



Hi! I'm going to use the LDC evm (I had it already) like a wear debris sensor. I want to register small wear debris in fluid flow. I suppose the fluid with debris will flows through L-tank (in plastic tube, for example). The velocity of flow is around 2 m/s. The diameter of debris is around 50um and larger. Also I hope, that I can to determine a material of debris (magnetic/ nonmagnetic for example).

Do you think it's really?