Other Parts Discussed in Thread: LM94023, LM94022
Hi,
Our customer would like to use the LM94023.
And they have a question about Temperature-Volgate Transfer Table(Table1).
The value of Vtemp(mv) in the table1 and the equation(1) results is different.
For example,in the case of Temperature=-50℃,GS=1
The Table is 1955mV , but the equation(1) is 1962mV.
Please let me know which is correct.
Best Regards,
Kato / Japan disty