This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Capacitive load for lm94023.

Other Parts Discussed in Thread: LM94023

Hi,

We plan to use LM94023 and I notice in the datasheet that there is some limitation concerning the capacitive load. If I understood, no series resistor is need if capacitive load is less than 1100pF. But a minimum series resistor must be placed if the capacitive load is higher, I suppose to limit the output current of the sensor...

But in that case I was expecting that the minimum recommended Rs would increase with capacitive load (since Rs max is 0 ohms for C<1100pF). But in the table it seems that the Rs minimum decrease from 3 kohms to 800ohms, while the Cload increase ?   Is it a stability problem ?