Hi,
There is a short description of the VCOM pin in the datasheet of TDC1000, "...note that the inputs of the LNA, PGA and comparators should be biased to the VCOM pin’s potential." I want to know to to do it exactly.
I asked this question, because I encountered some problems. I failed to get any STOP pulse even if I set the ECHO_QUAL_THLD to 0h (-35mV), and saw the echo signal peak on the COMPIN reached far blew the threshold (Vpp > 500mV).