I am evaluating the TMP107 for a current project and purchased the TMP107EVM.
I have looked at the following documnets:
SBOA138A ( Easy-to-use Cabling Interface for Measuring Temperature with the TMP107)
SBOS716B (TMP107 Digital Temperature Sensor with Bidirectional UART One-Wire Interface and EEPROM) and
SBOU158 (TMP107EVM User's Guide).
I am not sure of how and when to use/program the EEPROM.
In the SBOS716B document 7.5.1 states the EEPROM is used to program and store values for writable registers, such as the configuration,...
Based on the above, I would expect the EEPROM to be unlocked ( per 7.5.2.1 of SBOS716B document) before a write to the
configuration register can take place.
However in Application report SBOA138A in 2.1, I do not see any 'unlocking' of the EEPROM prior to writing to the configuration register
for demonstrating the continuous conversion mode (A) and the shutdown mode (B).
Are there any software examples or other application notes or accompanying code composer projects using the TMP107 with say an MSP432 microcontroller
Thanks