Because my system needs higher power for the ultrasonic transducer, I need to drive the transducer with higher voltage.
I came up with following ideas driving transducer with 10V peak to peak voltage.
a) High = 10V, Low = 0 V
b) High = 5V, Low = 0V
Method a) works with negative connection tied to ground, and positive connection oscillating between 0V and 10V.
Method b) works without negative connection tied to ground. Rather, both negative and positive connection is driven with 5V high and 0V low oscillation, but with 180 degree phase shifted resulting in POS-NEG oscillating between (-5V ~ +5V).
Is there difference between the two methods? Or Does it depend on transducers?
Thank you.