Hello,
I am using the LDC1051 in an application which the circuit board it is mounted to can be disconnected from the system while powered, and re-connected to a hot circuit. This of course causes potentially harmful transients on the board. The connector which mates this board and connects the SPI lines from the sensor to an off-board microcontroller has all of its lines protected with TVS diodes and capacitors at the connector. Unfortunately the LDC1051 can randomly become damaged after "hot plugging" it's circuit board into the system. The failure mode is a "resistive" short on VDD.
A few questions:
1. Are there any pins on the IC that may be more sensitive to transients than others?
2. Can I ground the No Connect pins? If not, should they be protected with TVS/capacitor?
3. Do you have any recommended guidelines for protecting this part from transients?
Thanks,
Kris Panaro