This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Booster board for the TDC1000-TDC7200EVM?

I know there is a booster board that takes a 5V output and steps it up to 30V for the TDC1000-GASEVM, but is there a booster board for the TDC1000-TDC7200EVM?


I would just purchase the TDC1000-GASEVM but the spec sheet says it's optimized for something like 150-300kHz and I need at least 1MHz. It's also stated that the GASEVM has resistors missing to step up the voltage. So I have to use the TDC1000-TDC7200EVM, but was wondering if there's a booster board that could be used or is specific for the TDC1000-TDC7200EVM. Can the booster board can be purchased separately or can the TDC1000-TDC7200EVM can be modified to use the booster board?

Much Appreciated,

John