Other Parts Discussed in Thread: LDC1612, LDC1614, LDC1101, TM4C1292NCPDT, MSP430F5528
I'm looking to build a sensor array using multiple MSP430's connected via SPI to multiple LDC1000's. These will be interconnected via some kind of high-speed communication like RS485 to forward selected data to a master controller which will assemble it into TCP packets on an ethernet connection to another machine which will perform the analysis.
I have ordered some MSP430F5529LP launchpads, and I have 5 LDC1000QEVM's which I plan to break apart and connect to the launchpad(s), have installed CCS and GCC, and the updates.
So I'm looking to see what software resources TI has to get me going - something for SPI access to configure and acquire data from the LDC1000's, and hopefully some kind of master/slave RS485 communications functionality to relay the data from the MSP430's to the ethernet concentrator (which will be another TI processor).
Also, is there a way to have a phone conversation with an FAE? I don't know what is usual and customary nowadays, 25 years ago it was standard to have an FAE assigned when we started a new project like this - is it still done that way?
Thank you.
Steve Freyder
Systems Engineer
Transcore
Plano, TX.