Although I opened a thread asked about it, I open this thread to avoid mixing questions.
We wanna design an industrial metal detector for under coveyor belt placement and i have any questions. The detection coils will be 2 sizes (160x600mm and
160x800mm).
1- With LDC1000 i can detect L (metal) and Rp (type of metal), and with LDC161X i can detect L only. Is this correct? On the other hand, with LDC161X i can get
more detection range and it can drive a lower Rp coil. It is not an absolute requirement, but I would detect type of metal.
2- What kind of coil can be better, PCB or air wire coil? Or 1 rectangular coil of 160x600, multiple array of 160x160 coil...., I hope I explained correctly.
3- Can the mechanical enclosure be metallic (the coils are placed into the metallic enclosure, with open aperture on top of the enclosure) or not? If i put a ferrite
sheet under the coils to improve detection range?
I have a LDC1000 kit and I´m waiting a LDC1614 kit + LDCCOILEVM for testing, although I have to make my own coils.
Any suggestions would be welcome.