This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP461 supply voltage

Other Parts Discussed in Thread: TMP461

Hello.

I 've been designed the board with TMP461.

In the TMP461 datasheet,  I think it can use 1.8V supply power.

If I want to use between other 1.8V device and TMP461 without level shifter, it can be possible?

According to the dataheet, "The TMP461 device operates with a power-supply range of 1.7 V to 3.6 V. The device is optimized for operation

at a 3.3-V supply but can measure temperature accurately in the full supply range."

it seems some limitations at device, when do not use 3.3V supply power.

Please, let me know the fact what is correct in operating condition.

Thank you.