I just wasted 2 days stuck with the LDC1000 EVM reading full count of 32768 all the time
It was working nice to start with then I added another coil of a bently necanada proximity snesor
I changed Rpmin and Max then pressed save after I did this the second time i thought the sensor was broken becauset the LDC1000 just kept giving 32768 full count all the time.
Just wanted to say thankyou to TI staff for this post
The problem was the sensor messsed up when saving registers for the second time just read 32768 full scale for proximity all the time.
I was using
GUI 1.0.4.1
Firmware 0.3.0.0
Driver EVM
after changing RPmin and Rpmax registers twice to suit my new coil it screwed up and constantly read 32768 proximity all the time
To get it workingafter many hours I followed the post linked above
Now set up is
GUI 1.0.3.0
Firmware 0.2.0.8.txt
LCD100EVM driver for usb
Its all working again now but I dare not alter the registers Rpmi and RPmax using the GUI to suit my new coil last time I did this it ruined the sensor and just read 32768 max proximity all the time.
Eventually I will snap the Sensor off the MPS40 Mvu Eval kit and interface it to my own PIC MCU using SPI and then display the proximity reading to a serial port.
Do you have to initialise all the registers on power up or does the LDC1000 have internal EEPROM and will remember the register settings which were set using the GUI ? Or so you have to initialise all the registers at power up VIA SPI evfery time then poll the Proximity data register to read the proximity as in distance from metal target to the coil sensor attached to ldc1000