Hi,
1. I want to measure the temperature of LEDs. I want to place the LM71 next to the LED and want to connect the Pad of the LED with the PAD of the LM71. The PAD of the LED is connected to 5V. Now I want to know if this is possible? I cant find any informations in the Datasheet of the LM71 if there is an electrical connection between the Pad and the die.
2. Also I dont undestand what means no pull back in this sentence: the 6-pin WSON (no pull back) package.
3. Also I dont understand the Soldering Information. How should I get a chip with a pad on a board with these specs?