Hi Expert,
I have checked several threads, it is said that HDC1080 can humidity result can settle right after power up.
My customer has developed 5 boards with HDC1080 on them. We found the humidity can only be settled to final accurate results after 120s.
e.g:
1. Power up the 2 boards with HDC1080 as reference, the humidity is 57%.
2. Power up the 3rd board, the initial humidity is 67%.
3. Waiting 2 minutes, the humidity decreased to 57%, kept stable.
They use the default register setting REG 0x02: 0x1000.
If there any thing can lead to slow response time?
Thanks a lot.
Zhou