Other Parts Discussed in Thread: LM95172-Q1
Hello,
We use the LM76 in some automatic test equipment. It is calibrated by curve fitting using a reference thermometer accurate to 0.02 deg C – target resulting accuracy of +/- 0.25 deg C. Temperature range -70 to +100 deg C. 20 temperature points in the calibration process (every 10 degrees +100 to -30 deg C, then every 5 degrees from -40 to -70 deg C). Process takes about 15 hours as great measures are taken to ensure temperature stability prior to taking measurements.
There is a recurring phenomenon whereby the error curve has a step around -40 to 45, the trend of which is maintained as temperature gets colder. In repeated tests, the magnitude of this step varies (0.05 to 0.2 deg C), sometimes barely visible, but more often than not it is there. This step has significant impact on the resulting curve fitting. The repeatability factor is also of concern obviously.
Looking into a number of possible causes, but wanted your opinion please.
We are aware of the following note in the datasheet: “Accuracy of the LM76CHM-5 will degrade 0.08°C for a ±1% variation in +VS from the nominal value.” Once we rule out any issues with the reference temperature probe used, we will perform some measurements on VCC. But this is an unlikely cause as the 5V supply is external to the thermal chamber, at room temperature. A power glitch could however still be related to connectors in the system.
Here are some sample datecodes, not sure how recent our stock is on this part:
M8RA
MSAB
Your help would be much appreciated!
Thanks,
Michel