Hi,
We are having issues stopping our OPT9221 based camera cleanly. Currently the camera is stopped by writing 1 to tg_dis (we do also drive the READY pin low, though though I don't think that would do anything adverse), then software resetting the chip. Nothing else is done to stop the stream. After 2-3 times of successfully starting, streaming data, then stopping, the OPT9221 appears to stop though the LEDs are still modulating; no further comms are possible over i2c after that and a hard reset is required to bring the chip back to life.
Is this something anyone has come across? This behaviour has only started since we switched from the OPT9220 to the OPT9221, is a different stop sequence required?
Thanks
- Oliver