This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-TDC7200EVM: Ultrasonic Sensing Forum

Part Number: TDC1000-TDC7200EVM


Hello,

  1)     My metal tank is 1m height and <100 cm width is it required that i should mount two piezo transducers to the tank ??? so that i can get accurate measurement ,should i require two or more than two ???if  two is the case then i shoud use two tdc1000-7200 evm modules??

2) Now ,I want to connect sim 900 (gprs module) for my set up for providing internet so that i can able to fetch my data and send the data to my dash board via cloud.Is this possible with tdc 1000-7200 module????

Thanks ,

Murali.