Dear Texas Instruments team,
I am searching for an accurate, sensible and user-friendly system to measure skin temperature in long distance runners during a controlled training session performed on treadmill. According to the information provided in your website, your temperature sensor “LMT70/LMT70A” may fit my goal. However, there are some questions I would like to ask you:
Are the LMT70/LMT70A sensors disposable or reusable?
Which other components other than the LMT70/LMT70A sensors does the system need to work properly (e.g. analog-to-digital converter (MSP430?), sensors charger, micro controller unit (still MSP430?), software for data analysis, etc.)? Since the LMT70 Evaluation Module includes 1 LMT70 and 1 MSP430, should I assume these 2 components are all what the system needs to work?
Can the sensor be directly placed and fixed to the skin with a normal tape or do they have specific requirements? Are they sweat-resistant?
Since I will also use a wi-fi electromyography system during the running measurements, is there a risk of cross-talk between the two devices?
I would be grateful if you could clarify the above-mentioned points.