Part Number: LDC1000EVM
Other Parts Discussed in Thread: LDCCOILEVM, LDC1101
I am using the coils provided by LDCCOILEVM with the LDC1000EVM.
How to properly set up sensor frequency and C for each one of this coils?
I know that I have to use this formula:
.
I know that f_sensor has to be between 5kHz and 5MHz.
1) How to choose the value of L for each coil of LDCCOILEVM from the datasheet?
2) Should I have to see this value of L when no target is close to the coil?
3) Which one between f_sensor and C have I to choose in order to determine the other?