I was planning to use the LM92 to measure skin temperature in a kneebrace. The goal of my project is to measure the temperature change after surgery. I found that the temperature after surgery rises between 0°C and 4°C. My question is whether the given accurancy of max +-0.33°C is a fixed value for each sensor, or if this value changes everytime I measue the temperature?
For clarification, if I measure every second, will my values allways be +0.20°C higher than the real temperature for example or will the values be +0.20°C on second one and -0.15°C at second two... In the last case is the difference between the two measurements 0.35°C wich is very high if there is only a rising between 0°C and 4°C.
With kind regards,
Pieter