Other Parts Discussed in Thread: LM71,
Hello,
Can you confirm if the LM71* and LM95071* devices are "100% compatible" at the software driver level?
I consider adding LM95071* as additional source to the LM71* that we currently use, and need to confirm interchangeability between the two in our 3.3V,SPI applications.
From what I read, only significant difference will be better accuracy from the LM95071.
Thank you!
Gilbert