Other Parts Discussed in Thread: PGA460, , BOOSTXL-PGA460
Hi,
I'm using PGA460 to measure the distance and I had a problem while using 200kHz transducer. The transducer that I'm using here: https://www.steminc.com/PZT/en/air-transducer-200-khz
Schematic:
Below is some images that I measured signal on the transducer output (P41 in schematic).
You can see in the echo dump data figure that it's hard to detect where is the echo pulse.
I've use the same circuit (with different value of C43 and C44) with 40kHz transducer and I can detect the echo pulse to detect the distance but it doesn't meet our requirement so we decide to try with 200kHz transducer but no luck. We don't think the problem come from the hardware since we can use with the 40kHz and 58kHz tranducer. Why would this happen?
another question is, is there any issues i put C43 and R41 in this way (CR) instead of RC?
Hope to hear from you soon. Thank you so much.
Thanks and best regards,
KH