This is for the current sensing forum which is not an option on the dropdown menu.
I have two INA220EVM modules and would like to use them simultaneously from the same PC host.
I have a previous post INA220EVM: USB Communication Error. in which I concluded that using legacy address was the only way to get my INA220EVM to work on the USB bus. Now I have a second EVM and launch the EVM app twice. I'm changing jumpers 4 and 5 to try a different address but I only get valid output from one EVM. The only mention of using multiple EVMs that I see in the manual is in the description of Jumpers 4 and 5 on the DIG board.