This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Connection issues over serial

Part Number: IWR1443

Hello everyone, 

I've been developing with the IWR1443 mmWave EVM for the past two weeks.

The software I've written was able to interface with the board over serial wonderfully, however, at the moment I am unable to connect to the board with my software or the mmWave Visualizer demo nor do the com ports for uart and data show up in the device manager.

We've had some of our technicians test the USB data pins with an oscilloscope while the board is connected to PC and it seems to no longer be talking to the PC at all. The board has been temperamental in regards to connecting with the PC since we've had it. I'm wondering if there is a technical fix or if we could get a replacement board from TI so that we can continue development? 

Thanks in advance, 

Dexter Banham

PS: We've tried different machines, cables, power supplies etc and nothing seems to help.  

[unlocked 1/19/18]>LE