Part Number: TMP411
we are looking to use this device for measuring temperature from an on chip Thermal Diode. The device can be supplied using 3.3V but for the I2C interface - we need to pull the SCL, SDA lines to 2.5V not 2.7V as recommended. Can this be done - we note that that Vih(min) for this device is 2.1V so we should be ok. If this is not possible - can you recommend an alternative device which can run off 2.5V?
thanks