This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: Failed to connect serial port when I want to do Flash Program in Radar studio 1.7.4.0

Part Number: AWR1243
Other Parts Discussed in Thread: UNIFLASH,

Hi,

I want to burn the spi flash of AWR1243 ES1.0 EVM by radar studio. I am using the radar studio 1.7.4.0 in DFP 07.

I first set the SOP = mode 5 in radar studio and it works ok. Then I tried to connect the serial port and got below error.

[09:35:43] [RadarAPI]: ar1.Connect(24,921600,1000)

[09:35:45] [RadarAPI]: Error: Connection failed: Calling_ConnectTarget returned 3

If I set the SOP = mode 2, I can connect the serial port well in radar studio.

Would you pls help?