This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: how to connect a 10 Pin or 14 Pin JTAG?

Part Number: AWR1642


Q1: Below is a standard TI 14 Pin JTAG. If I want to connect 14Pin JTAG to AWR1642, PD(Vcc) is connected to 3.3V, how I can deal with the TCK_Ret, EMU0, EMU1?

Q2: Can we use a 10 Pin JTAG? If use it , can I connect it like the figure below? 

Thanks very much.