hello
in document of AWR1243 Cascading, Said for Digital frame timing synchronization, The SYNC_OUT pin of Master connect to Slave's SYNC_IN and for avoid of delay feed back into Master's SYNC_IN.
1-Is it necessary to connect Master's SYNC_IN to external processor which now connected to Master's SYNC_OUT to avoid delay?
2-Is it necessary to connect Master's SYNC_OUT to external processor? or can not use of this pin for SOP(Sense On Power)? need to use 47.5K resistor which said in datasheet?
3- If cascading circuit is not considered and we want to use single AWR1243 chip, can we not connected Master SYNC_IN and SYNC_OUT to external processor?
Thank for your attention.