Other Parts Discussed in Thread: LDC1312,
Hello Eveyone,
I'm using the LDC1312 EVM to designing a new kind of Inductive Sensor. I have my own coil with L = 2260 uH and the capacitor to create the tank circuit is C = 3,3nF. The oscillation frequency in this case is about 58KHz. When I aproximate the target (stainless steel) close to the coil the frequency increase to about 224KHz, but the signal is too noised, like the drawing below.
I added the commom shokew filter like the recomendation of datasheet with four 33pF capacitors and a SRF3216 inductor the impedance match. The results were not too good because the signal continued noised.
Do you have any ideias to decrease the noise? Maybe I have to implemente a digital filter in firmware or no?
Thank you very much
Best Regards