Other Parts Discussed in Thread: DRV401, DRV421, DRV411, DRV421EVM, TPS7A19, TL720M05-Q1
Hello,
According to DRV401-Q1 overview material, it is designed for VAC sensor.
Does it mean that DRV401-Q1 can only be used with VAC sensor?
If DRV401-Q1 can be used with other sensors,
1. Can you support Sensor matching like as Input/Output information and Magnetic core information?
2. Can DRV401-Q1 support over 300A rated current? Can you recommend Turn ratio and etc
3. Can you recommend Icom1 & Icomp2 output spec between Compensation coil and Compensation driver ?
Regards,
Nicky