This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: how to design the antenna to the max azimuth ±20 degree

Part Number: AWR1642


Hi,

    The azimuth scope of AWR1642 is  ±60 degree,now we want to develop the AEB((Autonomous Emergency Brake) system,and the azimuth scope is  too large for our system.To satisfy our need, the max azimuth should be  ±20 degree and the max range 120m.

1.Can you provide the suitable tecnical solution to meet our performance requirement?

2. If we design the antenna on our own, because we are new in antenna design,can you provide some tecnical support for antenna design?

Thanks in advanced,

Regards,

Rata