I am reading in "Programming Chirp Parameters in TI Radar Devices" (SWRA553) about the timing constraints for chirps on the AWR devices, and I would like to validate some of my chirp configurations to make sure the idle/ADC start/ramp end times are valid. The document mentions the ramp timing calculator in Radar Studio, and I'd like to be able to use it. However, it appears that Radar Studio will not start properly unless you have a TSW400 installed and connected to your computer. I do not have a TSW400, but the timing calculator would still be useful to me and doesn't need to depend on connected hardware. Is there any way I can run this tool without a TSW400?
I expect that someone will suggest using the mmWave Sensing estimator. This does not accomplish the same thing, as you cannot enter arbitrary chirp parameters directly. You are limited to computed parameters based on the constraints you enter.