Other Parts Discussed in Thread: LM339
Firstly, thanks for your time and attention.
We are using the LM35DT/NOPB attached to a heatsink and soldered onto a PCB. We have noticed intermittent failures similar to failure mode 1 in the original thread "High failure rate with hand-soldered LM35 TO-92".
Our unit performs a power on self test and sometimes an over temperature condition is detected. What is perplexing is that the failure happens very infrequently but it happens in clusters so that we may power cycle the unit 4 or 5 times in a row with it failing each time with an output that is too high to be a real temperature( 1.2V ) and then it will power up and pass on the next POST. We recently ran almost 5000 power on/off cycles without seeing any failures. Has TI ever observed a power up behavior like this? Could a transient voltage between Ground pin and the TO220 tab during power on cause this?
Regards,
Barry