Part Number: TDC1000-TDC7200EVM
Other Parts Discussed in Thread: TDC1000, TDC7200
Tool/software: TI C/C++ Compiler
Hi!
I am integrating a RF95 wireless module on the same SPI bus as the TDC1000 and TDC7200 as a slave. The module could only handle max 10MHz of CLK so I needed to divide it by 4 (UCB0BR0) to get 6MHz instead of 12MHz, which worked.
However I am afraid that it could affect the TOF measurement timings of the TDC1000/7200 communications. What are side affects of slowing CLK down? (using it for flow metering).
I had one idea of changing the frequency depending of which slave that is used, would that be a good idea? If so, do I need to shutdown the SPI bus every time I change it?
Thanks in advance!
Regards,
Thibault