This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8241: Is is possible to design a ToF Camera system of an outdoor working range about 10m with OPT8241 and OPT9221?

Part Number: OPT8241

Dear TI,

I am planning to design a ToF Camera system that of a working rage about 10m with OPT8241 and OPT922, so I am reading TI documents and design reference guide regarding ToF cameras. 

I understood the working range related to the modulation frequency. Also the enery of the modulated light is propotional to the illumination power. The illumination power attenuates as the distance increases. The environment of this application is outdoor, sometimes with rain, fog, snow and direct sunshine.

Does TI also provide the other necessary components (illumination board, lens,lens holders and so on) to enable a fast integration of a system?  

Looking forward to your reply.

Best Regards

Luyuan