This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01000: People Counting Lab - recording camera frames

Part Number: TIDEP-01000

Hi there

I have successfully completed the people counting tutorial for the IRW1642BOOST EVM - I can run the visualiser with all the intended functionality - however I would like to be able to save the output from the camera feed for analysis at a later point. Is this possible and if it is then would I be able to get some guidance on how to do this, please? 

Thanks in advance.

Alistair

  • Hi Alistair,

    Currently, our GUI does not support saving the webcam video.  Your webcam should have some support for capturing video itself.  To capture clips with the GUI and the webcam video synchronized, I use OBS. It is free and open source. You can configure OBS to record multiple windows at the same time, and set the location of these windows in the video.

    Regards,

    Justin