Dear Technical Support Team,
Do you have the information of failure mode?
When failure mode occurs , what does LM20 output(High or Low or HIz or open)?
Best Regards,
ttd
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Technical Support Team,
Do you have the information of failure mode?
When failure mode occurs , what does LM20 output(High or Low or HIz or open)?
Best Regards,
ttd
Hello,
I will have to check with our design engineers on this question. I will get back with you as soon as I get a response.
Thank you and regards,
Audrey
Hi Audrey,
LM20 is analog output device below figure.
Does it have cmos gate logic on output?
If it is yes, could you show the structure of it?
■Datasheet
Shutdown capability for the LM20 is intrinsic because its inherent low power consumption allows it to be powered directly from the output of many logic gates or does not necessitate shutdown.
Best Regards,
ttd
Hi,
According to the datasheet, the LM20 is an analog CMOS output device. Since this is a dated part, I do not have the information on-hand about the structure of the output. I am consulting our design team to see if they have more information on this.
Thank you,
Audrey