Other Parts Discussed in Thread: LMT01, TMP117, TMP107, TMP112, LM335
What is the maximum load capacitance for the LM335A?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Stern,
There isn't a max capacitance load limit in the datasheet. However, I don't think capacitive load is an issue for the device since its output stage is just the zener output + resistor.
-Kelvin
Dear Kelvin:
Less than the allowed maximum.
Perhaps there is a chart of series resistance vs. capacitive load for stability?
Regards,
Mark
Dear Kelvin:
I am using the die version of this device, LM335A MDC.
I will provide filtering into an ADC.
Is it OK to simply add, for example, a 0.1uF (or other) cap across the output or is a resistor in series with the cap advisable?
If the unit is at the end of a cable, is this a problem?
Any guidance concerning stability criteria would be welcome.
Regards,
Mark
Mark,
I will forward the information to our designer.
For any analog signal chain, you will have to consider noise interference. Especially for a long cable. The solution for these types of problems are not unique to analog temperature sensors. Generally, you want to shield and limit bandwidth by filtering, which can be costly. Thus, that's why I proposed that you should consider our digital sensors like TMP117/TMP112/LMT01/TMP107.
Are you making a probe?
-Kelvin
Mark,
Please refer to pg. 32 for Bob Pease's comment on LM335. He basically said that 0.1uF+22ohm is fine. The article also pointed out a way to validate the stability empirically if you're interested in other cap values.
Bob Pease Lab Notes Part 7.pdf
Unfortunately, since this is an old part we can't simulate the original design to give you a general recommendation of capacitive load vs isolation resistor requirement. Your best course of action forward is by empirically testing the stability of the circuit as describe in Bob's article.
-Kelvin