Part Number: LM94023
Hello dear Sensing Team,
I have a question regarding the LM94023 temperature accuracy. I would like to know, what accuracy degree can be achieved, minus the calculated nonlinearity of the MCU. Can the accuracy be improved, when applying the linear approximation, mentioned on the p.11 of the datasheet?
Or is the linear approximation already included in the following values?
Temperature Accuracy:
-20°C to 40°C ± 1.5°C
-50°C to 70°C ± 1.8°C
-50°C to 90°C ± 2.1°C
-50°C to 150°C ± 2.7°C
BR