This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IVC102: Question on timing for S1 S2

Part Number: IVC102

Hello,

I'v got a question regarding the timing of the two switches S1 and S2. I wont to use the IVC102 wit a variable integration time. I will do the following:

  • apply sensor signal by closing S1
  • wait until  output of the IVC201 reaches a defined value, using a comparator, and count the time
  • then open S1
  • wait for time 1 (holding time in the data sheet)
  • close S2
  • wait for 10µs to discharge the integrator
  • open S2
  • wait time 2 (pre integration time in data sheet)
  • open S1 for next cycle

Now my question, I'd like to make the time 1 and time 2 as small as possible. When I have a look on  the slew rate of the amplifier the data sheet says 3v/µs. so my max. output voltage will be arround 2V, so would it be OK, if time 1 and time 2 are 1µs?

Kind regards

Guido