This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: Do I need to use CAN FD interface?

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: MMWAVE-SDK, DCA1000EVM, MMWAVE-STUDIO

Hello,

I have one AWR1642BOOST and want to do target recognition algorithms verification. Is it possible that I get L3 radar cube data through modifying the demo project code? should I use CAN FD interface? Because I was warned before UART rate is quite low and CAN is a better interface to send out the object data, which is much faster than UART. Thanks a lot!

Kind regards,

Kathy