Hello,
I want to use the DRV5055, in a combination with a microcontroller, as a magnetic field zero-cross detector. That's why I'm interested in the behavior of the quiescent output voltage. The datasheet shows a range from 2.43V to 2.57V (5V supply voltage) and that's my first question: Is it possible to measure the quiescent voltage during production line and store this as an offset, or will the offset be different after every restart of the sensor? Maybe you can sketch the internal structure to get a better understanding of how the quiescent voltage will be generated or the reason for this massive offset range.
Another point is the temperature related drift of the quiescent voltage, this is specified with +/-1% of VCC, which means +/-50mV for 5V operation. Is it right to add both differences to get the maximum output error? Than the worst case would be +/-70mV as initial error and +/-50mV as temperature related error, so overall +/-120mV?
Regards
Christian