This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMT87: Do we have a part which can measure lower than – 38 Degree Celsius at 3.135 V?

Part Number: LMT87


Hi Sensor Team,

my customer is using LMT87.

By powering LMT87 with 3.3 V – 5 Per Cent = 3.135 V, max neg. temperature which can be measured is – 38 Degree Celsius.

 

Do we have a part which can measure lower than – 38 Degree Celsius at 3.135 V?

 

Thank you,

kind regards,

Marion