This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/LDC1312EVM: TTY commands?

Part Number: LDC1312EVM
Other Parts Discussed in Thread: LDC1312

Tool/software: Linux

I'm trying to talk to the EVM via a terminal.  I did get minicom to connect and once I got a response from the MSP430, but I have no idea what I actually sent to get that response.

The interface-protocol is AT-Commands, but nothing seems to actually get any kind of response.  Is there any documentation that describes what commands are used to set the registers inside the LDC1312?  If it is really a modem interface, is there a baud rate it wants set in the terminal?

Thank you for any help.

Mike