Other Parts Discussed in Thread: OPT3101, , PGA460-Q1, PGA460
Hi,
In a factory automation application we are trying to measure a varying distance between a moving object and a fixed heavy metal (steel) plate. We must attach the sensor to the moving object. The distance to be measured varies between 0 and 25mm. We can also add an offset up to 60mm....this means the measured range can be 60 to 85mm. The measurement resolution sought is 0.1mm or better
We have considered OPT3101 EVM and we have been advised by TI that this would not be able to satisfy our need.
We have been advised that TDC7201 is a direct time of flight sensor while OPT3101 is indirect because it measures phase shift rather than directly the time for light to travel there and back) so the technology is a bit different.
The question is can TDC7201-EVM satisfy our need?
If not do you have a TOF product that can?
Regards
Sam