Other Parts Discussed in Thread: TIDEP-01006, IWR6843, , IWR1443BOOST, IWR1443, TMDSEVM572X
Tool/software: Linux
In TIDEP-01006, the dependencies between the required hardware and software are not clear. So I want to know the validated combination of the hardware and software.
I guess that the validated combination of hardware and software is as follows.
[Validated mmwave hardware]
- IWR6843ISK (IWR6843 ES1.0)
- IWR1443BOOST (IWR1443 ES3.0)
[Validated processor hardware]
- TMDSEVM572X Rev.A3a
[Validated software]
- mmWave SDK v03.01.00.02 (The support for IWR6843 is provided starting from version 03.01.00.02)
- Linux Processor SDK v05.02.00.10 (Add IWR6843 (60GHz) support to the TI design TIDEP-01006)
- Ubuntu 14.04.5
- ROS Indigo Igloo (Release date: July 22nd, 2014)
Is my guess correct?
Best regards,
Daisuke