Hi Team,
Customer has a question need your help.
After the ADC_EN_VREF bit is set, TOP_TON outputs 2.5v. Clearing the TEST_MUX_DAC_EN bit, but it does not "Connects DAC output to TOP/TON pins", which is still 2.5V.
Base on the material:
- TEST_MUX_P_EN bit is cleared. Connects PGAIN output to TOP/TON pins
- TEST_MUX_T_EN bit is cleared. Connects TGAIN output to TOP/TON pins
- TEST_MUX_DAC_EN bit is cleared. Connects DAC output to TOP/TON pins
Are the three digits cleared at the same time and all connected to TOP/TON pins? Not interlocking?
Thanks.