Part Number: OPT3101
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Getting started
Training videos: https://training.ti.com/zero-hero-time-flight-training-series
Device datasheet: http://www.ti.com/lit/ds/symlink/opt3101.pdf
Evaluation
OPT3101EVM is available here: http://www.ti.com/tool/OPT3101EVM Device is pre-calibrated and ready for use. EVM demonstrates using OPT3101 for long range single channel ToF distance measurements.
TIDA010021 is a reference design demonstrating OPT3101 used for wide field-of-view with multiple zones of detection. It is available here: http://www.ti.com/tool/TIDA-010021
System level design (component selection and board design)
System design involves optical component selection and board design and layout. The system design guide provides all the necessary theory and instructions for this process. The estimator tool helps with selecting optical emitters and photodiodes and estimating performance, range, and accuracy for these components.
system design guide: https://www.ti.com/lit/an/sbau305b/sbau305b.pdf
system estimator tool: http://www.ti.com/tool/OPT3101ESTIMATOR-SW
Calibration
Tools
The SDK tool provides all C++ functions needed for calibration. This can be integrated to an existing system or run on any host with C++ compiler (microprocessor, linux PC, windows, etc.). It can also be used in calibration tool mode on a TI MSP430 launchpad to speed calibration process which requires no coding and simply commenting a line of code per calibration step and compiling the code in Code Composer Studio. Details of this method are run through step-by-step in the SDK user guide document included in the SDK.
SDK: http://www.ti.com/tool/OPT3101-SDK
The configurator tool is a graphical interface for selecting the OPT3101 settings to use for the design. It generates an SDK configuration file with register settings that can be imported to the SDK and eliminates the need to select individual register settings.
Configurator tool: http://www.ti.com/tool/OPT3101CONFIG-SW
Documents
How to calibrate doc: http://www.ti.com/lit/pdf/slau791
Register level calibration doc: http://www.ti.com/lit/pdf/sbau310
App notes
We have a number of app notes that give more details on a variety of topics. These are available here: http://www.ti.com/product/OPT3101/technicaldocuments#doctype1
Overview of collateral
http://www.ti.com/product/OPT3101#design-resources-for-you
E2E FAQs