This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101: waveform configuration

Part Number: LDC1101


Dear friends, 

I am now working with STM32F103-LDC1101. 

After configuring the LDC1101, I found that the output waveform is not similar to the datasheet. 

Here is the output waveform from INA and INB. 

Please help me to configure the LDC1101 to generate the output waveform similar to EVM. 

Thank you

Here is my setting for SPI: 

void SPI_CLOCK_Configuration(void)
{
    GPIO_InitTypeDef GPIO_InitStructure;
    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
    GPIO_InitStructure.GPIO_Pin = GPIO_Pin_8;
    GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
    GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
    GPIO_Init(GPIOA, &GPIO_InitStructure);

//    GPIO_PinAFConfig(GPIOA, GPIO_PinSource8, GPIO_AF_0); 
    RCC_MCOConfig(RCC_MCO_HSE); //Sets MCO to 8 MHz
//    RCC_MCOConfig(RCC_MCO_SYSCLK); //Sets MCO to 8 MHz
//     __disable_interrupt();
//     __enable_interrupt();
}

void SPI_Configuration(void)
{
  uint32_t Div = 2;
  uint32_t DivVal = 0;
  GPIO_InitTypeDef GPIO_InitStructure;
  SPI_InitTypeDef SPI_InitStructure;
  RCC_ClocksTypeDef Clk;
// Init LCD IOs and SPI1  
  RCC_APB2PeriphResetCmd(  RCC_APB2Periph_GPIOA
                         | RCC_APB2Periph_GPIOB
                         | RCC_APB2Periph_SPI1
                         | RCC_APB2Periph_AFIO,
                           DISABLE);
  RCC_APB2PeriphClockCmd(  RCC_APB2Periph_GPIOA
                         | RCC_APB2Periph_GPIOB
                         | RCC_APB2Periph_SPI1
                         | RCC_APB2Periph_AFIO,
                         ENABLE);
  // Deinitializes the SPI1
  SPI_I2S_DeInit(SPI1);
  /* Configure SPI_MASTER pins: SCK and MOSI ---------------------------------*/
  GPIO_InitStructure.GPIO_Pin = SPI_MASTER_PIN_SCK | SPI_MASTER_PIN_MOSI;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP;
  GPIO_Init(SPI_MASTER_GPIO, &GPIO_InitStructure);
  /* Configure SCK and MOSI pins as Alternate Function Push Pull */  
  GPIO_InitStructure.GPIO_Pin = SPI_MASTER_PIN_MISO;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN_FLOATING;
  GPIO_Init(SPI_MASTER_GPIO, &GPIO_InitStructure);
  /* Configure SPI pins : NSS4 */
  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_4;
  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP;
  GPIO_Init(GPIOA, &GPIO_InitStructure); 
  /* SPI1 no remap (NSS/PA4, SCK/PA5, MISO/PA6, MOSI/PA7) */
  GPIO_PinRemapConfig(GPIO_Remap_SPI1, DISABLE);
  
  /* SPI_MASTER configuration ---------------------------*/
  SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex;
  SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
  SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b;
  SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;
  SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
  SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
  SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_64;
  SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
  SPI_InitStructure.SPI_CRCPolynomial = 7;
  SPI_Init(SPI_MASTER, &SPI_InitStructure);

  /* Enable SPI_MASTER TXE and RXNE interrupt */
//  SPI_I2S_ITConfig(SPI_MASTER, SPI_I2S_IT_TXE, ENABLE);
// SPI_I2S_ITConfig(SPI_MASTER, SPI_I2S_IT_RXNE, ENABLE);

  // Clock Freq. Identification Mode < 4MHz
  RCC_GetClocksFreq(&Clk);

  while ((MAX_SPI_FREQ * Div) <= Clk.PCLK1_Frequency)
  {
    Div <<= 1;
    if (++DivVal == 7)
    {
      break;
    }
  }

  SPI1->CR1 = (SPI1->CR1 & ~(0x7 << 3)) | ((DivVal&0x7) << 3);

  // Enable SPI1
  SPI_Cmd(SPI1, ENABLE);
}
void SPI_write(uint8_t addr, uint8_t data) 
{
  addr = addr & 0x7F; // The MSB is a 0-write register, which is a 1-read register
  LDC_CS_LOW;
  delay_a(1);

    while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
    SPI_I2S_SendData(SPI1, addr); // send 8Bit address
    while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
    SPI_I2S_SendData(SPI1, data); // send 8Bit 8bit data
    while (SPI1->SR & SPI_I2S_FLAG_BSY);  
    
  LDC_CS_HIGH;
  delay_a(2);  
}

uint16_t SPI_read(int8_t addr)
{
    static uint8_t data=0;
    addr = addr | 0x80; // The MSB is 1-read register
    
  delay_a(5);
  LDC_CS_LOW;
  delay_a(2);
  
    // address bits
    while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
    SPI_I2S_SendData(SPI1, addr);// send Address
    while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));
    SPI_I2S_ReceiveData(SPI1);
    // data bits
    while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
    SPI_I2S_SendData(SPI1, 0x00);
    while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));
    data = SPI_I2S_ReceiveData(SPI1);

    while( SPI1->SR & SPI_I2S_FLAG_BSY );
    
    delay_a(2);
    LDC_CS_HIGH;
    delay_a(5);  

    return data; 
}
#include "stm32f10x.h"
#include "LDC1101.h"
#include "LDC1101_CMD.h"
/* Global variable----------------------------------------------------*/
uint32_t LHR_DATA;
uint16_t RP_DATA;
uint16_t _responsetime; // Response Time
uint8_t _divider;       // divider
uint16_t _LHRoffset;    // LHR_OFFSET
float _RPmin;           // RP_MIN
float _RPmax;           // RP_MAX
float _fsensor;         // f_sensor: the calculated frequency of the sensor
float f_sensor_min = 5E+5;

float _fCLKIN = 8E+6;          // f_CLKIN: frequency of external clock: 16MHz
float _cap = 42E-9;             // capacitor: 120 pF
uint16_t _Rcount = 0x1F29;       // The reference count - 1kSPS 0x1F29



/*----------------------------------------
Function: LDC write register
Function parameters: 
                    addr: register address
                     dat: data
----------------------------------------*/
void writeSPI(uint8_t dat , uint8_t addr)
{
//  uint16_t tmp=0;
//  uint32_t i = 0;
  
  addr = addr & 0x7F; // The MSB is a 0-write register.
//  tmp = ((uint16_t)addr << 8) | dat;
  LDC_CS_LOW;
  delay_a(1);
    
  // address bits
  while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
  SPI_I2S_SendData(SPI1, addr);
  // data bits
  while (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) == RESET);
  SPI_I2S_SendData(SPI1, dat);
  while( SPI1->SR & SPI_I2S_FLAG_BSY );

  LDC_CS_HIGH;
  delay_a(2);  
}


/*----------------------------------------
Function: LDC read register
Function parameters: 
                    addr: register address
----------------------------------------*/
uint8_t readSPI(int8_t addr)
{	
  static uint8_t data=0;
//  uint16_t tmp = 0;
  addr = addr | 0x80; // The MSB is 1-read register
//  tmp = ((uint16_t)addr << 8);
  delay_a(5);
  LDC_CS_LOW;
  delay_a(2);
  
  // address bits
  while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
  SPI_I2S_SendData(SPI1, addr);
  while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));
  SPI_I2S_ReceiveData(SPI1);
   // data bits
  while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE));
  SPI_I2S_SendData(SPI1,0x00);
  while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE));
  data=SPI_I2S_ReceiveData(SPI1);
  
  while(SPI1->SR & SPI_I2S_FLAG_BSY);

  delay_a(2);
  LDC_CS_HIGH;
  delay_a(5);  
  
  return data; 
}

Here is my setting for LDC1101: 
void func_mode(LDC_MODE mode) { // Sleep mode writeSPI(mode,0x0B); // delay(0.8); } void setRPmode( void ) { writeSPI( 0x02, 0x05 ); // ALT_CONFIG: 0000 0010 --> RP modus + Shutdown enabled writeSPI( 0x00, 0x0C ); // D_CONFIG: Enables LHR modus, disables RP } void setLHRmode(void){ writeSPI(0x01,0x05); writeSPI(0x01,0x0C); } void setResponseTime(LDC_RESPONSE responsetime) { static uint16_t resps[] = {0, 0, 192, 384, 768, 1536, 3072, 6144}; _responsetime = resps[responsetime]; // uint8_t DIG_CONF; // DIG_CONF = readSPI(0x04); // writeSPI(( DIG_CONF & 0xF8) + responsetime, 0x04); writeSPI(responsetime, 0x04); } void setReferenceCount(uint16_t rcount) { _Rcount = rcount; uint8_t LHR_RCOUNT_LSB = (rcount & 0x00ff); uint8_t LHR_RCOUNT_MSB = ((rcount & 0xff00) >> 8); writeSPI(LHR_RCOUNT_LSB, 0x30); //LSB writeSPI(LHR_RCOUNT_MSB, 0x31); //MSB } void set_fsensor_min(void) { // uint8_t DIG_CONF; // DIG_CONF = readSPI(0x04); // uint8_t MIN_FREQ = 16.0f - (8.0f / f_sensor_min); // writeSPI(((MIN_FREQ << 4) + (DIG_CONF & 0x00)), 0x04 ); writeSPI(0x00,0x04); } void setRPsettings(bool RP_MAX_DIS, RPMAX rpmax, RPMIN rpmin) { static float rps[] = {96, 48, 24, 12, 6, 3, 1.5, 0.75}; _RPmin = rps[rpmin]; _RPmax = rps[rpmax]; writeSPI((RP_MAX_DIS << 7) | (rpmax << 4) | rpmin, 0x01); } void setDivider(DIVIDER div) { static uint8_t divs[] = {1, 2, 4, 8}; _divider = divs[div]; writeSPI(div, 0x34); } void setLHRoffset( uint16_t offset ) { _LHRoffset = offset; uint16_t LHR_OFFSET = offset; writeSPI((uint8_t) (LHR_OFFSET & 0x00ff), 0x32 ); // LSB writeSPI((uint8_t) ((LHR_OFFSET & 0xff00) >> 8), 0x33 ); // MSB } void sleep(void) { /* stop toggling the CLKIN pin input and drive the CLKIN pin Low */ func_mode( LDC_MODE_STANDBY ); } void wakeup(void) { /* start toggling the clock input on the CLKIN pin */ init(); // delay(0.5); } void init_LDC1101(void) { /********* SETTINGS ***************** ** C_sensor = 120 pF ** L_sensor = 5 uH ** Rp_min = 1500 Ohm ** ** RCount = 65535 (max) ** Samplerate = 1 kHz ** t_conv = 1 ms ** ** f_sensor_min = 6.4 MHz (d = inf) ** f_sensor_max = 10 MHz (d = 0) ** divider = 1 ************************************/ // Set LDC1101 in configuration modus func_mode( LDC_MODE_STANDBY ); // STANDBY = 0x01 naar 0x0B // - initialise LHR mode & enable SHUTDOWN mode setLHRmode(); // LHR mode // setRPmode(); // RP+L modek // - set ResponseTime to 192 // setResponseTime( LDC_RESPONSE_192 ); // - set LHR_Rcount to highest resolution(LHR) setReferenceCount( _Rcount ); // - set calibrated value for f_sensor_min (d = inf, no target) // set_fsensor_min(); // minimum 500kHz // - disable RP_MAX // - set RP_MIN to 1,5 kOhm (RPMIN_1) setRPsettings( 1, RPMAX_0, RPMIN_1 ); // LHR mode // setRPsettings( 0, RPMAX_96, RPMIN_1 ); // RP+L mode // - set Divider to 1 (for large range / ENOB / resolution) setDivider( DIVIDER_1 ); // - shift the signal down a bit setLHRoffset( 0x00 ); // Done configuring settings, set LDC1101 in measuring modus func_mode( LDC_MODE_ACTIVE ); } void LDC_Init() { // Set LDC1101 in configuration modus func_mode( LDC_MODE_STANDBY ); // STANDBY = 0x01 naar 0x0B writeSPI(0x36, LDC1101_CMD_RP); writeSPI(0xDD, LDC1101_CMD_TC1); writeSPI(0xFD, LDC1101_CMD_TC2); writeSPI(0xD7, LDC1101_CMD_DIGCONFIG); writeSPI(0x00, LDC1101_CMD_ALTCONFIG); writeSPI(0x00, LDC1101_CMD_THRESHILSB); writeSPI(0x00, LDC1101_CMD_THRESHIMSB); writeSPI(0x00, LDC1101_CMD_THRESLOLSB); writeSPI(0x00, LDC1101_CMD_THRESLOMSB); writeSPI(0x00, LDC1101_CMD_INTB_CONFIG); writeSPI(0x00, LDC1101_CMD_D_CONFIG); writeSPI(0x00, LDC1101_CMD_LTHRESHLSB); writeSPI(0x00, LDC1101_CMD_LTHRESHMSB); writeSPI(0x00, LDC1101_CMD_LTHRESLLSB); writeSPI(0x00, LDC1101_CMD_LTHRESLMSB); writeSPI(0x68, LDC1101_CMD_STATUS); writeSPI(0x00, LDC1101_CMD_RP_DATA_LSB); writeSPI(0x00, LDC1101_CMD_RP_DATA_MSB); writeSPI(0x00, LDC1101_CMD_L_DATA_LSB); writeSPI(0x00, LDC1101_CMD_L_DATA_MSB); writeSPI(0x29, LDC1101_CMD_LHR_RCOUNT_LSB); //0xFF writeSPI(0x1F, LDC1101_CMD_LHR_RCOUNT_MSB); //0xFF writeSPI(0x00, LDC1101_CMD_LHR_OFFSET_LSB); writeSPI(0x00, LDC1101_CMD_LHR_OFFSET_MSB); writeSPI(0x00, LDC1101_CMD_LHR_CONFIG); writeSPI(0x00, LDC1101_CMD_LHR_DATA_LSB); writeSPI(0x00, LDC1101_CMD_LHR_DATA_MID); writeSPI(0x00, LDC1101_CMD_LHR_DATA_MSB); // Done configuring settings, set LDC1101 in measuring modus func_mode( LDC_MODE_ACTIVE ); } float get_fsensor_min() { uint8_t DIG_CONF; DIG_CONF = readSPI(0x04); return (float) 8.0f/(16.0f - (float) ((DIG_CONF& 0xf0) >> 4)); } bool is_New_LHR_data(void) { return(!(get_LHR_status() & 0x01)); } bool is_Oscillation_Error(void) { return(get_status() & 0x80); } uint8_t get_status(void) { uint8_t status; status = readSPI(0x20); return status; } uint8_t get_LHR_status(void) { static uint8_t LHR_status; LHR_status = readSPI(0x3B); // ERR_ZC: (LHR_status & 0x10) >> 4 // // ERR_OR: (LHR_status & 0x08) >> 3 // // ERR_UR: (LHR_status & 0x04) >> 2 // 1 = LHR_DATA < 0 because LHR_OFFSET > LHR_DATA // ERR_OF: (LHR_status & 0x02) >> 1 // // LHR_DRDY: (LHR_status & 0x01) // 1 = Data ready return LHR_status; } //float get_Q(void) //{ // return _RPmin * sqrt(_cap/_inductance*1000000); //} float get_fsensor( uint32_t Ldata ) { static float _Ldata; _Ldata =(float)Ldata; // LHR mode if( Ldata == 0 ) { _Ldata = get_LHR_Data(); } _fsensor = _fCLKIN * (float)_divider * (_Ldata + (float)_LHRoffset*256)/16777216; // (p.26) // RP+L mode // if( Ldata == 0 ) { Ldata = get_L_Data(); } // _fsensor = (_fCLKIN * 6144) / (3 * Ldata); // (p.31) return _fsensor; } /* GETTING DATA FROM SENSOR-------------------------------------------------- */ uint16_t get_RP_Data(void) { RP_DATA=0; LDC_CS_LOW; // address bits while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); SPI_SendData8(SPI1, 0x80 | 0x21); while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); SPI_ReceiveData8(SPI1); // data bits while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); SPI_SendData8(SPI1, 0x00); while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); RP_DATA += ((uint16_t)SPI_ReceiveData8(SPI1)); // data bits while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); SPI_SendData8(SPI1, 0x80 | 0x22); while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); RP_DATA += ((uint16_t)SPI_ReceiveData8(SPI1))<<8 ; // writeSPI(ADG); while( SPI1->SR & SPI_I2S_FLAG_BSY ); LDC_CS_HIGH; return RP_DATA; } float get_RP( uint16_t RPdata ) { static float _rp; // if( RPdata == 0 ){ // RPdata = get_RP_Data(); // } _rp=_RPmin * (1.0f - ((float) RPdata / (65535.0f-1.0f))); //return (_RPmax * _RPmin) / ( _RPmax * (1.0f - ((float) RPdata / 65535.0f)) + _RPmin * ((float) RPdata / 65535.0f)); return _rp; } uint32_t get_LHR_Data(void) { LHR_DATA=0; LDC_CS_LOW; // address bits while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); SPI_I2S_SendData(SPI1, 0x80 | 0x38); while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); SPI_I2S_ReceiveData(SPI1); // data bits while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); SPI_I2S_SendData(SPI1, 0x00); while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); LHR_DATA += ((uint32_t)SPI_I2S_ReceiveData(SPI1)); // data bits while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); SPI_I2S_SendData(SPI1, 0x80 | 0x39); while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); LHR_DATA += ((uint32_t)SPI_I2S_ReceiveData(SPI1))<<8 ; // data bits while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)); SPI_I2S_SendData(SPI1, 0x80 | 0x3A); while(!SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)); LHR_DATA += ((uint32_t)SPI_I2S_ReceiveData(SPI1))<<16 ; // writeSPI(ADG); while( SPI1->SR & SPI_I2S_FLAG_BSY ); LDC_CS_HIGH; return LHR_DATA; } float get_Inductance( uint32_t Ldata ) { static float _inductance; // the calculated inductance _fsensor = get_fsensor( Ldata ); _inductance = 1/(_cap * 4*PI*PI*_fsensor*_fsensor); // (p.34) return _inductance; } // Delay ms void delay_a(uint32_t nCount) { uint32_t index = 0; for(index = (nCount*1); index != 0; index--) ; }